Technical FAQs

Ask a Question

Is the SC8L125S provided with a factory installed service disconnect?

No, the service disconnect(s) must be field installed in this device. Install only HOM type of breaker, 125A maximum. Only (1) 125A HOM breaker can be installed, and is limited to the top position only. All other (3) positions are limited to 100A maximum. A maximum of (4) HOM breakers can be installed.

CTA-ID : 2030583
Was this helpful?
What can we do to improve the information ?