Technical FAQs

Ask a Question

What is the coupler for the LJB810? Does it come with the straight piece?

Coupler p/n is LJB8C. The straight piece does come with the connectors as standard. The bag is inside the straight piece. It includes the gasket, sealing plate, nuts and bolts and instruction sheet.



CTA-ID : 2030546
Was this helpful?
What can we do to improve the information ?