Technical FAQs

Ask a Question

Are approval drawings available for the Individual Meter Sockets and the Horizontal Gang Meter Sockets?

Issue:
Product Design Drawings

Product Line:
Individual meter sockets and Horizontal Gang Meter Sockets

Environment:
CAD Drawings

Cause:
Application

Resolution:
Approval drawings for these devices can be obtained, BUT since Square D does not manufacture these particular products, a drawing might need to be requested from the supplier. For approval drawing availability for individual meter sockets, please contact the Lexington Product Support Group @ the email address = lexpsg@schneider-electric.com or call 888-Squared (888-778-2733) and select Option #1, Option #1 and Option #5.

 
Was this helpful?
What can we do to improve the information ?