Technical FAQs

Ask a Question

What is the IP rating for the XY2CH/XY2CE cable Pulls?

It is IP65 conforming to IEC529, IP657 conforming to NF C20-010(IP667 with booted push button)


CTA-ID : 2030553
Was this helpful?
What can we do to improve the information ?