Technical FAQs

Ask a Question

What components are used in an FHE26000A?

The FHE26000A consists of a FHL26000M molded case switch factory installed in a (modified) FA100A enclosure. The enclosure markings are modified to indicate that the device is an enclosed molded case switch, not an enclosed circuit breaker.



CTA-ID : 2030851
Was this helpful?
What can we do to improve the information ?