Technical FAQs

Ask a Question

Can a KAL36200 and JDL36200 circuit breaker be mounted in same enclosure?

Issue:
Product design feature

Product line;
Circuit breaker enclosures

Environment:
Circuit breakers

Cause:
Application or availability

Resolution:
No. These two breakers would have separate catalog number enclosures and the enclosures would NOT be UL listed for both breakers to be used in that same enclosure. The KAL breaker is obsolete and no longer available and the JDL is the current Power Pact J frame that can ONLY be used in the J Frame enclosures listed in the current digest.


 
Was this helpful?
What can we do to improve the information ?