Technical FAQs

Ask a Question

What is the length of the shaft on the 9001K70, 72, 30, 32, 34 and 36 Joystick Operators with a latch?

It is 2.91 inches from the face of the panel to the tip of the operator handle.

CTA-ID : 2030635
Was this helpful?
What can we do to improve the information ?