Technical FAQs

Ask a Question

Can a Class R Fuse Kit, once installed in a fusible General Duty safety switch, be removed?

Issue:
Product design features

Product Line:
Heavy Duty Safety Swithces

Environment:
Accessories

Cause:
Application

Resolution:
No, the concept of the Class R fuse kits is for safety and are not designed to be removed from the switch they are installed. 


CTA-ID : 2030700
Was this helpful?
What can we do to improve the information ?