Technical FAQs

Ask a Question

3013302650, what voltage is this coil?

Since the pilot light is powered by an induction coil, the coil voltage (control voltage) is NOT restricted to 120VAC which means it can be used with ANY coil voltage. This pilot light coil is designed to be used with a 6 volt lamp such as a GE44.




CTA-ID : 2030673
Was this helpful?
What can we do to improve the information ?