Technical FAQs

Ask a Question

Is the SC816D150C provided with a factory installed service disconnect?

Yes, a HOM2150 is supplied factory installed. The factory installed HOM2150 feeds the 8 space/16 circuit loadcenter interior. Additional space is provided for the field installation of a second HOM main breaker, 50A maximum.

CTA-ID : 2030612
Was this helpful?
What can we do to improve the information ?