Technical FAQs

Ask a Question

Is the SC8L125F provided with a factory installed service disconnect?

No, the service disconnect(s) must be field installed in this device. Install only HOM type of breaker, 110A maximum. A maximum of (4) HOM breakers can be installed.


CTA-ID : 2030585
Was this helpful?
What can we do to improve the information ?