Technical FAQs

Ask a Question

Is there a mounting difference between the K frame and the Powerpact H frame in an I-Line panel?

In 3 pole applications they are both 4.5``. In 2 pole applications, the K frame is 4.5`` and the Powerpact H frame is 3``.


CTA-ID : 2031267
Was this helpful?
What can we do to improve the information ?