Technical FAQs

Ask a Question

What components are used in an LHE26000AWK?

The LHE26000AWK consists of a LHL26000M molded case switch factory installed in a (modified) LA400AWK enclosure. The enclosure markings are modified to indicate that the device is an enclosed molded case switch, not an enclosed circuit breaker.



CTA-ID : 2030771
Was this helpful?
What can we do to improve the information ?