Technical FAQs

Ask a Question

What is the terminal lug data for the DTU366 Double throw safety switch and are there alternate lugs?

Issue:
Product Design features

Product Line:
Double Throw Safety Switches

Environment:
Lug wire size

Cause:
Installation

Resolution:
The lugs on this switch will accept (2) 250-500kcmil Al/Cu.

There are NO alternate lugs for this switch

 
Was this helpful?
What can we do to improve the information ?