Technical FAQs

Ask a Question

What is the part number for a 8 Circuit Nema 3R Pre Wired Generator Panel?

Nema 3R Pre Wired Generator Panels are not available. Suggested using a QO816L100RB, 2-QO260 (if requirement is for 60 ampere mains), and a QO2DTIM Mechanical Interlock Attachment with Retaining Kit. This will provide a balance of (4) 1-pole QO mounting spaces, capable of (8) 1-pole, 20 ampere maximum circuits if using QOT tandem breakers.

CTA-ID : 2030539
Was this helpful?
What can we do to improve the information ?