Technical FAQs

Ask a Question

Is the deadfront for a NQOD20M100 mounted on the interior or the can?

It is mounted on the interior.


CTA-ID : 2031052
Was this helpful?
What can we do to improve the information ?