Technical FAQs

Ask a Question

What are dimensions of the MHL361200 breaker?

The dimensions on the MAL/MHL 1200 A breaker is the same as the 300A - 1000A with only the lugs being different. Instead of the AL900MA lug it has the AL1000MA lug.


CTA-ID : 2031241
Was this helpful?
What can we do to improve the information ?