Technical FAQs

Ask a Question

What are the repair parts for a PAK72C, Series E02, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Cover - 4054025101
Cover Mounting Screws - 2142717161 (2 req`d)
Interior Trim - 4054541701
Interior Trim Mounting Screw - 4020513001K (2 req`d)
Interior Assembly - (2) 4054009150 and 4055331450 (Includes the Base Assy, Circuit Breaker(s) and Receptacle(s) listed below. Also includes the neutral assembly, not listed separately)
Interior Assembly Mounting Screw - 2142217101 (4 req`d)
Base Assembly - 4054006850
Circuit Breaker - (2) QO120GFI and QO220
Receptacle - (2) 4054001450 (125 volt/20 amp) and 4054004351 (125/250 volt/20 amp)
Receptacle Mounting Screw - 2190312160 (1 req`d for each 125 volt/20 amp receptacle, 2 req`d for the 125/250 volt/20 amp receptacle)
Neutral Bonding Strap Assembly - 4054017250
Ground Bar - 4023017155
Ground Bar Mounting Screw - 4020547201 (1 req`d)
Closing Cap - BCAP
Closing Cap Mounting Screw - 2142720241
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 2031187
Was this helpful?
What can we do to improve the information ?