Technical FAQs

Ask a Question

Are the option cards and serial communications cards for the ATV58 CSA approved?

Yes the ATV58 and all of its options (VW3A58****) are CSA approved.



CTA-ID : 2015351
Was this helpful?
What can we do to improve the information ?