Technical FAQs

Ask a Question

Is there a small liquid level switch suitable for hazardous locations?

No, The 9034 LLV56 (Digest 173 page 20-19) is rated Hazardous location Class I, Groups A, B, C, D: Class II Groups E, F, G, Class III. This product is now obsolete and no direct replacement.

CTA-ID : 2031085
Was this helpful?
What can we do to improve the information ?