Technical FAQs

Ask a Question

Is the C4L200S provided with a factory installed service disconnect?

No, the service disconnect(s) must be field installed in this device. Install only (2) QO type of breaker, 100 ampere maximum.


CTA-ID : 2030581
Was this helpful?
What can we do to improve the information ?