Technical FAQs

Ask a Question

Can a second 200 ampere main service disconnect be added to the SU3040D300FB?

No, it cannot. Additional space is provided for the field installation of a second QDL main service disconnect, 100A maximum.

CTA-ID : 2030662
Was this helpful?
What can we do to improve the information ?