Technical FAQs

Ask a Question

Is the CU816D400CB provided with a factory installed service disconnect?

Yes, a QDL22200 is supplied factory installed. The factory installed QDL22200 feeds the 8 space/16 circuit loadcenter interior. Additional space is provided for the field installation of a second QDL main breaker, 200A maximum.

CTA-ID : 2030560
Was this helpful?
What can we do to improve the information ?