Technical FAQs

Ask a Question

Are MP Meter Pak devices available with alternate physical layout configurations?


Product Line:
MP Meter Pak

Alternate layout

No alternate physical layout configurations are available. For specific requirements concerning the physical layout, consider the EZM Meter Center product line. Using EZM products, the branch units can be installed either to the left or to the right side of the EZM main device.

CTA-ID : 2030788
Was this helpful?
What can we do to improve the information ?