Technical FAQs

Ask a Question

What is the replacement for a fuseholder for a MCT12B operating room clock timer? The old catalog number 2549909510 is now obsolete.

Issue:
Maintenance

Product Line:
PTEQP - LV EQPT (IEC & NEMA)

Environment:
NFPA99, NEC517.160

Cause:
The fuse holder may need to be replaced due to normal wear and tear.

Resolution:
Catalog number 2549909510 which was a red fuse holder, has been changed to catalog number 2549909550, which is a black one. Please note that the MCT12B is obsolete and has been superseded by the Iso-Gard IGT Dual Clock/Timer.


CTA-ID : 2030606
Was this helpful?
What can we do to improve the information ?