Technical FAQs

Ask a Question

Is the C125RB provided with a factory installed service disconnect?

No, the service disconnect must be field installed in this device. Install only QOM1-VH type of breaker, 125 ampere maximum.


CTA-ID : 2030575
Was this helpful?
What can we do to improve the information ?