Technical FAQs

Ask a Question

Is the CU12L400CB provided with a factory installed service disconnect?

Yes, a QDL22200 (200A) main breaker is supplied factory installed. Additional space is provided for the field installation of a second QDL main breaker, 200A maximum. Further additional space is provided for the field installation of up to four QOH main breakers, 125A maximum. The total ampacity of the combination of QOH breakers cannot exceed 200A. All of the breakers installed would be considered service disconnects.


CTA-ID : 2030566
Was this helpful?
What can we do to improve the information ?