Technical FAQs

Ask a Question

On an ``F`` frame circuit breaker FH36100S35 , what is the S35?

The ``S35`` is an old suffix. Thebreaker number is now FH3610035. The newer ``35`` suffix is a special factory calibration for the breaker to operate at 50 degrees C.

CTA-ID : 2031411
Was this helpful?
What can we do to improve the information ?