Technical FAQs

Ask a Question

9999SX6: What is the voltage and amperage rating of the contacts?

9999 SX6 is rated up to 600 v and 10 amp continuous.


CTA-ID : 2031405
Was this helpful?
What can we do to improve the information ?