Technical FAQs

Ask a Question

Can you open a disconnect switch on the output of the Altivar ATV66 drive while the motor is still running?

This is not recommended but can be done if the following conditions are met:
1) The disconnect switch must be ``load break rated``.
2) There is a minimum 1.5% inductor on the out put of the drive between the drive and the disconnect switch to limit the voltage feedback.


CTA-ID : 6973
Was this helpful?
What can we do to improve the information ?