Technical FAQs

Ask a Question

Is the RC2M200S provided with a factory installed service disconnect?

No, the service disconnect(s) must be field installed in this device. Install only (1) QOM2-VH type of breaker, 200 ampere maximum and (1) QO-VH type of breaker, 50 ampere maximum.

CTA-ID : 2030579
Was this helpful?
What can we do to improve the information ?