Technical FAQs

Ask a Question

Is the CM200S provided with a factory installed service disconnect?

No, the service disconnect must be field installed in this device. Install only QOM2-VH type of breaker, 200 ampere maximum.


CTA-ID : 2030576
Was this helpful?
What can we do to improve the information ?