Technical FAQs

Ask a Question

What is the HP range for the E-Flex drive at 208, 230 and 460 Volts?

The E-Flex drive is designed to be a cost effective enclosed drive controller solution for typical HVAC motor applications.
1 to 100 HP at 460/480 Vac.
1 to 50 HP at 208 & 230 Vac.
For motors outside this HP range and for features not available in the E-Flex drives, consider the M-Flex drives.

Reviewed 11/2011

CTA-ID : 2031121
Was this helpful?
What can we do to improve the information ?