Technical FAQs

Ask a Question

What are the catalog #s for TVSS 480 volt 3-phase 4-wire and 120/208 volt 3-phase 4-wire?<br /><br />

Refer to the Digest Plus Product Selector, available on-line at www.squared.com for selection. Digest section 6 has the TVSS information


CTA-ID : 2031357
Was this helpful?
What can we do to improve the information ?