Technical FAQs

Ask a Question

What is the rated voltage and current for a Merlin Gerin auxiliary switch catalog number 29450?

This auxiliary switch unit/contact block is rated for 6 A @ 600 Vac or 300 mA @ 380 Vdc.


CTA-ID : 2031390
Was this helpful?
What can we do to improve the information ?