Technical FAQs

Ask a Question

What does the term ``Multi-fixing`` mean regarding K cam switches ?

This indicates a switch operator that fixes itself in a door or cover with multiple screws ....generally 2 or 4 . Hence multiple mounting holes need to be drilled in the mounting surface in addition to the center hole for the shaft . This contrasts to a single hole ( generally 22mm diameter ) mounting method .

CTA-ID : 2031372
Was this helpful?
What can we do to improve the information ?