Technical FAQs

Ask a Question

What are the advantages of JDA36150 or HDA36150 over KA36150?

Powerpact H- and J- frame breakers are the new style of thermal magnetic circuit breakers and will replace KA, KH, and KC breakers - they offer field-installable accessories, interrupting ratings as high as 100kA at 480V, common footprints, mounting holes, and handle operators to standardize panel layouts from 15A to 250A.

CTA-ID : 2031295
Was this helpful?
What can we do to improve the information ?