Technical FAQs

Ask a Question

Is it permissible to change the 30 amp breakers in a QO generator panel catalog number QO48M30DSGP to a 40 amp circuit breakers?

Putting 40A breakers in the 30A device would compromise the UL listing of this generator panel. It is UL listed and tested for 30A breakers only.

CTA-ID : 2031239
Was this helpful?
What can we do to improve the information ?