Technical FAQs

Ask a Question

Can an AP30210 busway straight piece connect to an AP302G10 ?

No ...the AP302G10 has a special connector at the joint for the integral ground ..........so the two pieces are not compatible .


CTA-ID : 2030752
Was this helpful?
What can we do to improve the information ?