Technical FAQs

Ask a Question

Does a MA1000F or MA1000S circuit breaker enclosure provide the capability to padlock the circuit breaker in either the ON or the OFF position?

Issue:
Product Features

Product Line:
Circuit Breaker Enclosure

Cause:
Clarification of standard product features

Resolution:
The MA1000F and MA1000S enclosures provide a Handle Padlock Attachment, HPALM, packaged with the enclosure. This attachment can be field installed on the breaker to provide padlock capability. A LAL frame of breaker can be padlocked in the ON or OFF positions. A MAL frame of breaker can be padlocked in the OFF position only.

NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 2030643
Was this helpful?
What can we do to improve the information ?