Technical FAQs

Ask a Question

Where is the shunt trip on a JD breaker installed and can it be seen once installed?

It is installed under a cover and it cannot be seen from the outside. The cover needs to be taken off. .

CTA-ID : 2030395
Was this helpful?
What can we do to improve the information ?