Technical FAQs

Ask a Question

How do you adjust a 9013GHG2J25 set 60 to 80 down to 70 from 80psi?

Issue:      
 How do you adjust a 9013GHG2J25 set 60 to 80 down to 70 from 80psi?

Product Line:
Pressure Switches

Environment:
9013 Pressure Switches

Cause:
 How do you adjust a 9013GHG2J25 set 60 to 80 down to 70 from 80psi?
 
Resolution:

Always adjust the large spring first by turning CCW until cut-out goes from 80 psi to 70 psi. This should bring the increasing set point down to 70 psi and maintain the 20 psi differential.


CTA-ID : 2030343
Was this helpful?
What can we do to improve the information ?