Technical FAQs

Ask a Question

How is 3 phase in and 1 phase out accomplished on an EZML312225?

An EZM 3 phase In - 1 Phase Out device will have four horizontal busbars, delivering 3 Phase/4 Wire to it from a 3 Phase Main Device. Only two of the three phases, and the neutral, will be tapped by vertical bussing to each of the tenant meter sockets, providing 1 Phase/3 Wire to the tenants.

CTA-ID : 2030416
Was this helpful?
What can we do to improve the information ?