Technical FAQs

Ask a Question

What are the repair parts for a CU12L400FN, Series M01?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
Only the parts listed below are considered field replaceable.
Meter Cover - 4056250650 Also requires insulator and rivets noted below.
Meter Cover Insulator - 4056138202 and Rivets (2) 2430313190
Meter Cover Mounting Screw - 4020513001K
Load Center Cover - 4056258950
Load Center Cover Mounting Screws - (3) 2142217101
Utility Pullbox Cover - 4056232801 (Handles not included, see below)
Utility Pullbox Cover Handles - (2) 2940101103 and Rivets (8) 2430315290
Utility Pullbox Cover Mounting Screws - (2) 4020513001K and (3) Sealing Screws - X1299
Load Center Interior - 4056250750
Load Center Interior Mounting Screws - (2) 2142217101
Interior Deadfront Trim - 4056233001
Interior Deadfront Trim Mounting Screws - 4020513001K
Meter Base Assembly - 21324CD
Mounting Channel - 4056142003
Factory Installed Main Breaker - QDL22200
QDL Main Breaker Mounting Pan - 4056235201 and (4) 2142720140 Pan Mounting Screws
Utility Lug Mounting Hardware - 4056211850
Semi-flush Flange Kit - FK400 (Includes top endwall, top flange and two side flanges)
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2030283
Was this helpful?
What can we do to improve the information ?