Technical FAQs

Ask a Question

Which power terminals are used on a U Line for the single phase application.

Use the single phase control unit and wire the power to L1 and L3 and wire the motor load to T1 and T3.


CTA-ID : 2030241
Was this helpful?
What can we do to improve the information ?