Technical FAQs

Ask a Question

What is the part # of mounting hardware for a KAL breaker?

Use a 48117-145-50 which consists of four 10/32 x 3`` bolts. Check with Cedar Rapids Customer Service for availability .


CTA-ID : 2030228
Was this helpful?
What can we do to improve the information ?