Technical FAQs

Ask a Question

What is the AIC ratings for the CE Marked EDB breaker?

CE Marking is not a standard. Just a marking , like a passport. There are no IEC 947-2 capacity ratings for this breaker.


CTA-ID : 2029913
Was this helpful?
What can we do to improve the information ?