Technical FAQs

Ask a Question

What is the replacement bonding strap used in for the QON42MS400, 400 amp, single phase load center?

Issue:
Old Design repair parts

Product Line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The bonding strap part number is 80110-605-01 and it would require two mounting screws, part #80110-802-01.


CTA-ID : 2030119
Was this helpful?
What can we do to improve the information ?