Technical FAQs

Ask a Question

What is required to convert a HOM612L100RB main lugs load center to a 50 ampere main breaker load center?

Issue:
Product design features

Product Line:
Homeline load centers

Environment;
Conversion to main breaker

Cause:
Application

Resolution:
This load center is a "fixed main lug" load center. The only option to convert this panel to a main breaker device would be to back feed a 2pole, homeline branch breaker as the main. A HOM1RK Retaining Kit would be required for the back feed option. The back feed option will use 2 of the load centers 6 spaces.


CTA-ID : 2030136
Was this helpful?
What can we do to improve the information ?