Technical FAQs

Ask a Question

What is required to convert a HOM48L125GRB main lugs load center to main breaker load center?

Product design features

Product Line:
Homeline load centers

Conversion to main breaker



This load center is a "fixed main lug" device. The only option to convert this load center to a main breaker, would be to back feed a 2pole homeline branch breaker as the main. The HOM1RK Retaining Kit would be REQUIRED for the back feed option. The back feed option will use 2 of the load centers 4 spaces.

CTA-ID : 2030141
Was this helpful?
What can we do to improve the information ?